Technical FAQs

Ask a Question

What is the part number for a 30mm pilot light with only 24amp light module and What is it's current rating?

Product Line: 
30 mm operators


You have to customize the part for a LED light module at that rating. We used the 24-28 Vac/Vdc LEDs with a current rating of 0.011666.

The part numbers were:

Green- 9001KP35LGG31

Red- 9001KP35LRR31

White- 9001KP35WW31


Was this helpful?
What can we do to improve the information ?