Technical FAQs

Ask a Question

9001KN300 new version is not working with my older operators. The new version of the legend plate has a tab which prevents the legend from working with older operators/push buttons. What can I do?

Product Line:
30 mm operators

The tab can be filed down if ultimately neccessary, but it is reccomended to buy new operators that will work with the new 9001KN300.
Was this helpful?
What can we do to improve the information ?