Technical FAQs

Ask a Question

What is the replacement for a QOM2200 load center Main Breaker?

Load Center Main Breaker 

Product Line:
QOM2 Circuit Breakers

QO and Homeline Load Centers

Replacement of old Main Breaker

The QOM2200 was a main breaker used in older Load Centers. It only had a 10kA interrupting rating. The QOM2200 is obsolete and no longer available, but can be replaced by the QOM2200VH. The breakers are the same physical size adn the only difference is the QOM2200VH will have a higher (22kA) interrupting rating.
Was this helpful?
What can we do to improve the information ?