Technical FAQs

Ask a Question

How do you convert the contacts from NO to NC or vice versa on a 8501 Type X relay?

Issue:
How do you convert the contacts from NO to NC or vice versa on a 8501 Type X relay?

Product Line:
8501 Type X Relays - GIC Product

Environment:
US Product

Resolution:
With all wiring removed, unscrew the two cover screws.  Remove the cover from the unit.  Physically pullthe contact out and flip it upsid down.  Reinsert the contact upside down and replace the cover and screws.
 
Was this helpful?
What can we do to improve the information ?