Technical FAQs

Ask a Question

Does the ATV28 drive has Sinking Logic Input?

Issue:
Does the ATV28 drive has Sinking Logic Input?

Product Line:
ATV28 Drives

Environment:
All serial numbers for ATV28 Drives

Cause:
N/A

Resolution:
No, the ATV28 drives do not have Sinking Inputs. The feature was only added to its replacement drives such as the ATV31 and ATV312.

Was this helpful?
What can we do to improve the information ?