Technical FAQs

Ask a Question

What is the minimum and maximum operating temperatures for indoor and outdoor rated QED Switchboards?

Issue:
What is the minimum and maximum operating temperatures for our N1 and N3R rated QED Switchboards?

Product Line:
QED Switchboards sold and supported in the USA.

Environment:
Ambient temperature ratings

Cause:
Operating temperature

Resolution:
The temperature range is between -40 degree F (-40 degree C) and 185 degree F (85 degree C). 
 
Was this helpful?
What can we do to improve the information ?