Technical FAQs

Ask a Question

What is the username and password for Powerlink G3 webpages?

Issue:
What is the username and password for Powerlink G3 webpages?

Product Line:
Powerlink G3 Lighitng Control

Envrionment:
North Americal, Commercial Building Lighting Control

Cause:
An NF3000G3 has an internal webpage which can be accessed by entering the IP Address of the controller in a web browser on the LAN.  There is a page Setup tab on the page that allows one to program the controller.  This page requires a username and password.

Resolution:
The default username is "admin".  The default password "admin."    There is a link on the left side of the page where one can change the username or password.
Was this helpful?
What can we do to improve the information ?