Technical FAQs

Ask a Question

What are the dimensions of the 9991SFA11 NEMA 12/3R enclosure?

Issue:
What are the dimensions of the 9991SFA11 enclosure.

Product Line:
9991 NEMA 12/3R Enclosures

Environment:
Product Features 

Cause:
Dimensional information 

Resolution:
For use with Class 8502:

Width = 18.15"/461mm
Height = 9.24"/235mm
Depth = 31.50"/800mm

For use with Class 8536:

Width = 18.15"/461mm
Height = 9.58"/243mm
Depth = 31.50"/800mm
Was this helpful?
What can we do to improve the information ?