Technical FAQs

Ask a Question

What are the dimensions of the 9991SCA11 NEMA 12/3R enclosure?

Issue:
What are  the dimensions of the 9991SCA11 Nema 3R/12 enclosure?

Product Line:
9991 NEMA 12/3R Enclosures

Environment:
Nema starter/contactors and accessories

Cause:
Product features 

Resolution:

Width = 6.38"/162mm
Height = 8.53"/217mm
Depth = 12.75"/324mm
Was this helpful?
What can we do to improve the information ?