Technical FAQs

Ask a Question

What are the dimensions of the 9991SDW2 NEMA 4 oversized enclosure?

Issue:
What are the dimensions of the 9991SDW2 Nema 4 oversized enclosure?

Product Line:
9991 NEMA 4 Enclosures

Environment:
Product features 

Cause:
Dimensional information

Resolution:
Width = 14.88"/378mm
Height = 7.25"/184mm
Depth = 16.19"/411mm
Was this helpful?
What can we do to improve the information ?