Technical FAQs

Ask a Question

What are the dimensions of the 9991SFW11 NEMA 4 enclosure?

Issue:
What are the dimensions of the 9991SFW11 NEMA 4 enclosure?

Product Line:
9991 NEMA 4 Enclosures

Environment:
Dimensional Information 

Cause:
Product Features 

Resolution:
For use with Class 8502:

Width = 18.15"/461mm
Height = 8.77"/223mm
Depth = 32.21"/818mm

For use with Class 8536:

Width = 18.15"/461mm
Height = 9.58"/243mm
Depth = 32.21"/818mm
Was this helpful?
What can we do to improve the information ?