Technical FAQs

Ask a Question

What are the dimensions of the 9991SCW11 NEMA 4 enclosure?

Issue:
What are the dimensions of the 9991SCW11 NEMA 4 enclosure?

Product Line:
9991 NEMA 4 Enclosures

Environment:
Dimensional Information 

Cause:
Product Features 

Resolution:
For use with Class 8903, and Class 8502:

Width = 6.38"/162mm
Height = 7.13"/181mm
Depth = 13.19"/335mm

For use with Class 8536:

Width = 6.38"/162mm
Height = 7.81"/198mm
Depth = 13.19"/335mm
Was this helpful?
What can we do to improve the information ?