Technical FAQs

Ask a Question

What are the dimensions for the 9991LXG1 NEMA 1 enclosure?

Issue:
I need to know the dimensions of the 9991LXG1 enclosure.

Product Line:
9991 General Purpose Enclosures

Environment:
US Product Lines

Cause:
Can not find it in the Digest

Resolution:

Dimensions (in/mm):

A = 7.81/198
B = 12.69/322
C = 6.03/153
D = N/A
E = 1.09/28
F = 10.50/267
G = 1.09/28
H = 1.09/28
I = 5.63/143
J = 5.75/146
K = 1.09/28
L = 5.63/143
Was this helpful?
What can we do to improve the information ?