Technical FAQs

Ask a Question

What replacement coils are available for the LC1F500?

Issue:
What replacement coils are available for the LC1F500?

Product Line:
TeSys F-Line Contactors

Environment:
All Product Lines

Cause:
Can not find it in the Digest

Resolution:

For LX1 standard style coils (most common):

24VAC (40 - 400 hz) = Not Available
48VAC (40 - 400 hz) = LX1FK048
110VAC (40 - 400 hz) = LX1FK110
120AC (40 - 400 hz) = LX1FK110
208VAC (40 - 400 hz) = LX1FK200
220VAC (40 - 400 hz) = LX1FK220
240VAC (40 - 400 hz) = LX1FK240
277VAC (40 - 400 hz) = LX1FK280
380VAC (40 - 400 hz) = LX1FK380
415VAC (40 - 400 hz) = LX1FK415
440VAC (40 - 400 hz) = LX1FK415
480VAC (40 - 400 hz) = LX1FK415
600VAC (40 - 400 hz) = LX1FK600


For LX9 special coils:


24VAC (40 - 400 hz) = LX9FK910
48VAC (40 - 400 hz) = LX9FK917
110VAC (40 - 400 hz) = LX9FK925
120AC (40 - 400 hz) = LX9FK925
208VAC (40 - 400 hz) = LX9FK930
220VAC (40 - 400 hz) = LX9FK931
240VAC (40 - 400 hz) = LX9FK932
277VAC (40 - 400 hz) = LX9FK932
380VAC (40 - 400 hz) = LX9FK936
415VAC (40 - 400 hz) = LX9FK936
440VAC (40 - 400 hz) = LX9FK937
480VAC (40 - 400 hz) = LX9FK937
600VAC (40 - 400 hz) = Not Available







 
Was this helpful?
What can we do to improve the information ?