Technical FAQs

Ask a Question

Is there a polyester enclosure option for 8538SF combination starters?

Issue:
Is there a polyester enclosure option for 8538SF combination starters?

Product Line:
8538 Combination Starters

Environment:
US Product Lines

Cause:
Selection/Application 

Resolution:
There is no option for a NEMA 4X enclosure for the NEMA size 4 through NEMA size 6 combination starters. The only option is to use the stainless steel enclosure.
Was this helpful?
What can we do to improve the information ?