Technical FAQs

Ask a Question

Are push buttons for push button heads for 9007C limit switches still available

Issue:
Are push buttons for push button  heads for 9007C limit switches still available

Product Line:
9007C Limit Switch Accessories - GIC Product

Environment:
US Product

Cause:
These parts have not been obsoleted, but the older part numbers have changed.

Resolution:
Use the following part numbers to order pushbuttons for the 9007R type heads:

2358C6G3 - black - 1 3/8"
2358C6G2 - red - 1 3/8"
2358C6G6 - green - 1 3/8"
2358C6G8 - yellow - 1 3/8"
2358C22G2 - black - 2 1/4"
2358C22G3 - red - 2 1/4"
2358C22G6 - yellow - 2 1/4"
2358C22G8 - black - 2 1/4"
 
Was this helpful?
What can we do to improve the information ?