Technical FAQs

Ask a Question

Conduit entry size for 9001BW control stations

Issue:
What is the conduit entry size for a 9001BW control station?

Product Line:
9001BW control stations - GIC Product

Environment:
US Product

Cause:
This specification is only listed with the dimensions.

Resolution:
The conduit entry is a 1/2" - 14 NPT on the bottom of the enclosure.
 
Was this helpful?
What can we do to improve the information ?