Technical FAQs

Ask a Question

What is the minimum and maximum mounting depth of the VCCF* shaft?

Issue:
What is the minimum and maximum mounting depth of the VCCF* shaft?

Product Line:
Vario Manual Switches

Environment:
US Product Lines

Cause:
Can not find it in the Digest

Resolution:
The maximum mounting depth is 12.25" and the minimum mounting depth is 5.50"
Was this helpful?
What can we do to improve the information ?