Technical FAQs

Ask a Question

CSA file for XPS Safety Product

Issue:
What is the CSA file for XPS safety products?

Product Line:
Preventa Safety Products - GIC Product

Environment:
US Product

Cause:
This certification is necesary for certain environments.

Resolution:
The CSA file is 248779, class 3211-03, and covers the following products:
  • Safety modules Series Preventa Types XPS-AL, -AM, -AP, -AS, -AT, -AX, -AMF, -APF, -ASF, -BA, -BC, -CEN, -CEP, -DA, -ECM, -ECP, -FB, -NS, -OT, -PVK, -PVT and -VN followed by a four or five digit number, may be followed by Z, may be followed by P, HS, LS or T followed by a number, open type, input, 24, 48, 115/120 or 230V ac, 50/60Hz, or dc.
  • Devices for electrical monitoring and control systems, modules Series Preventa Types XPS-AC, -AF, -AFL, -AK, -AR, -ATE, -AV, -BF, -CM, -DMB, -DME, -MP, -TSA, -TSW, -VC and -VNE, followed by a four, five or six digit number, may be followed by HS, may be followed by P, may be followed by T with a three digit number, open type, input, 24, 48, 110, 115/120, 120 or 230V ac, 50/60Hz, or dc.
  • Modules Series Preventa, open type, Types XPS-MC, followed by 16 or 32, followed by X or Z, may be followed by C or P, input: 24V dc; output 24V dc 2A; pilot duty: 24V dc 1.5A (L/R 50ms), C300.  Maximum surrounding temperature: 55oC.
http://www.csagroup.org/us/en/services/testing-and-certification/certified-product-listing/certficate/248779%257C3211-03

 
Was this helpful?
What can we do to improve the information ?