Technical FAQs

Ask a Question

Do we have keyed switches with larger than 10A capacity?

Are there keyed selector switches which are capable of carrying greater than 10A?

Product Line:
9003K2 Cam switches - GIC Product

US Product

9001SK keyed operators are limited to 10A continuous

The 9003K2 cam switches can use a keyed operator.  They are UL listed for up to 12A continuous and VDE 0660 rated 16A.  The complete ratings are attached.
Was this helpful?
What can we do to improve the information ?