Technical FAQs

Ask a Question

What is the terminal lug data for the QMB368W?

Issue:
Product features

Product Line:
QMB

Environment:
Product features

Cause:
Clarification

Resolution:
The QMB368W is provided with 4 lugs per phase, each lug accept (1) #3/0 AWG - 600 KCMIL aluminum or copper conductor.
 
Was this helpful?
What can we do to improve the information ?