Technical FAQs

Ask a Question

Can the ATV71 accommodate two encoder cards?

Issue:
Can the ATV71 accommodate two encoder cards?

Product Line:
ATV71

Environment:
All models and serial numbers

Cause:
None

Resolution:
No, the ATV71 drive can only accommodate one encoder card.
Was this helpful?
What can we do to improve the information ?