Technical FAQs

Ask a Question

What is the largest branch breaker that will fit into the QON42M300 panel, will a 200A branch fit?

Issue:
What is the largest branch breaker that will fit into the QON42M300 panel?  Will the load center accept a  200A branch?

Product Line:
QON panels

Environment:
Selection, application 

Cause:
Is there a 200A branch breaker for the QON42M300 panel.

Resolution
The QO3100 is largest branch breaker that will fit into the QON42M300. No we do not offer a 200A branch breaker for the QON42M300 panel.

Was this helpful?
What can we do to improve the information ?