Technical FAQs

Ask a Question

What is the replacement knife switch on HU1003MC?

Issue:
Is replacement knife switch available on HU1003MC

Product Line:
Motor Control MCC4 disconnect switch

Environment:
Motor Control MCC4 discount switch

Cause:
Replacment knife switch

Resolution:
The knife switch is the line side assembly and this is not offered as a separate part. The entire  HU1003MC will need to be replaced.


 
Was this helpful?
What can we do to improve the information ?