Technical FAQs

Ask a Question

Do the QONQ load centers, catalog numbers QONQ42MS300 and QONQ42MS400 come with the main breaker already installed?

Issue:
Product feature

Product Line:
QO Load Centers

Environment:
QONQ Load Centers

Cause:
Clarification

Resolution:
Yes, the 300A and 400A QONQ load center comes with the main breaker factory installed.
Was this helpful?
What can we do to improve the information ?