Technical FAQs

Ask a Question

Do you offer buttons for the Type M manual starters that are labeled "On/Off" instead of "Start/Stop"?

Issue:
Do you offer buttons for the Type M manual starters that are labeled "On/Off" instead of "Start/Stop"?

Product Line:
2510 Type M Manual Starters

Environment:
US Product Lines

Cause:
Can not find an option for it in the Digest

Resolution:
No. We only have an option for "Start/Stop".
Was this helpful?
What can we do to improve the information ?