Technical FAQs

Ask a Question

Is the ATV71's available in IP54 ATV7W...?

Issue:
Are ATV71's available in IP54 ATV7W...?

Product Line:
ATV71  Altivar 71

Environment:
ATV71W

Cause:
Application need

Resolution:
No ATV71's are not available in ATV71W ( IP54).  Only the ATV61's were availabe with IP54 rating but the ATV61 series drives are discontinues as of 1/1/17.
Was this helpful?
What can we do to improve the information ?