Technical FAQs

Ask a Question

What is the terminal lug data and torque requirements for a H366DS?

Issue:
Product wire size and torque

Product Line: 
Heavy Duty Safety Switches

Environment: 
Lug wire data and torque specs

Cause: 
Installation 

Resolution: 

The H366DS will accept as standard (2) 3/0-500kcmil Al/Cu wires per phase and neutral and there are NO alternative wire sizes or range for this switch.
The torque specification for the Main Lugs is 375 lb-in  and is shown on the wiring diagram of the switch. 

 

Was this helpful?
What can we do to improve the information ?