Technical FAQs

Ask a Question

Do the 9007C limit switches have positive opening contacts (Direct acting contacts)

Issue:
Do the 9007C limit switches have positive opening contacts (Direct acting contacts)

Product Line:
9007C limit switches - GIC Product

Environment:
US Product

Cause:
Positive opening contacts are required for certain applications

Resolution:
Without modification, the 9007C limit switches are not positive opening.  The form code Y1561 can be used on some limit switches to provide a NC positive opening contact.  The complete description is as follows:
Y1561 - One pole, normally closed, slow-make slow-break, direct acting contact mechanism substituted for standard snap switch on types C52 and C54
 
Was this helpful?
What can we do to improve the information ?