Technical FAQs

Ask a Question

Difference between XCSA802 and XCSA803

What is the difference between the XCSA802 and the XCSA803?

Product Line:
Preventa Safety Switches - GIC Product

US Product

The XCSA802 is not available for purchase in the US but is installed on some equipment in the US

The XCSA802 and the XCSA803 are identical except for the conduit entries.  The XCSA802 has an M20 metric threading, while the XCSA803 is 1/2" NPT.  As previously stated, the XCSA802 is not available in the US.
Was this helpful?
What can we do to improve the information ?