Technical FAQs

Ask a Question

What is the valid part number for MS limit switches

Issue:
Why is the MS limit switch not coming up as valid in the system?

Product Line:
9007MS Miniature Limit Switches - GIC Product

Environment:
US Product

Cause:
These parts must be ordered correctly

Resolution:
Use the class number 9007 to preface the part number. For example, order 9007MS01S0100 instead of MS01S0100.
Was this helpful?
What can we do to improve the information ?