Technical FAQs

Ask a Question

What is the catalog number for the Altivar Process Drives?

Issue:
Where can the part numbers be found for the Altivar Process Drives (ATV630, ATV650, ATV930, ATV950 etc)?

Product Line:
Altivar Process Drives

Environment:
ATV630
ATV650
ATV930
ATV950

Cause:
Need documentation

Resolution:
The best resource for currently available part numbers is the Installation Manuals that are published on our website.

ATV630/650 Installation Manual:  http://www.schneider-electric.com/en/download/document/EAV64301/
ATV930/950 Installation Manual:  http://www.schneider-electric.com/en/download/document/NHA80932/

These manuals also include mounting, wiring, and installation information.
Was this helpful?
What can we do to improve the information ?