Technical FAQs

Ask a Question

Will the R2 run relay on the ATV312 drive still be close showing drive is running when the drive is in low speed time out mode?

Issue:
Will the R2 run relay on the ATV312 drive still be close showing drive is running when the drive is in low speed time out mode?

Product Line:
Alivar 312

Environment:
All

Cause:
Needs to know if the R2 run relay can open if the drive goes into the low speed timeout mode?

Resolution:
No if the drive still has a run command and the drive goes into low speed timeout the R2 run relay will remain closed even in sleep mode.
Was this helpful?
What can we do to improve the information ?