Technical FAQs

Ask a Question

What terminals are used on the E-flex enclosed drive to indicate run and fault status?

Issue:
What terminals are used on the E-flex enclosed drive to indicate run and fault status?

Product Line:
8839 E-Flex

Environment:
E-Flex only

Cause:
Needs to know where to land his run status and fault status on the E-flex drives.

Resolution:
The is one NO and NC contacts for Run status and one NO and NC contact for fault status.   Both contacts are dry and  you can find the contact ratings in figure 1 below.


                                                                              Figure 1
Was this helpful?
What can we do to improve the information ?