Technical FAQs

Ask a Question

What size mushroom buttons are compatible with the 9001KYG1Y?

Issue:
What size mushroom buttons are compatible with the 9001KYG1Y?

Product Line:
30mm operators

Environment:
US Product

Cause:
This is not specified in published literature

Resolution:
The control station is to be used with 30mm maintained mushroom head pushbuttons only.  The diameter of the mushroom head must be 40mm (1-5/8") or smaller to fit appropiately within the guard.
 
Was this helpful?
What can we do to improve the information ?