Technical FAQs

Ask a Question

Padlock guard for 9001SKR5R

Issue:
Is there a specific padlock guard for a 9001SKR5R?

Product Line:
30mm operators

Environment:
US Product

Cause:
There is no guard listed specifically

Resolution:
The 9001K4 can be used with this operator.  It is not listed because it will not be corrosion resistant (NEMA 4X) and the operator is.  Using this padlock will bring the NEMA rating down to NEMA 4. 
 
Was this helpful?
What can we do to improve the information ?