Technical FAQs

Ask a Question

Are there mounting holes in the 9001KYG1Y?

Issue:
Are there mounting holes in the 9001KYG1Y?

Product Line:
30mm Control Stations

Environment:
US Product

Resolution:
Yes, this unit has mounting holes in the same place as the standard 9001KYG1.  The mounting holes are 3.00" right to left and 2.75" top to bottom.  See the attached drawing for more specific information.
 
Was this helpful?
What can we do to improve the information ?