Technical FAQs

Ask a Question

What is the typical required VA rating on a a control transformer for combination starter?

Issue:
What is the typical required VA rating on a a control transformer for combination starter?

Product Line:
8538/8539 Combination Starters

Environment:
US Product Lines

Cause:
Can not find it in the Digest

Resolution:
See Table 16.104 on page 16-41 of the Digest 176. This sizing can also be used for other 8502 and 8536 based devices.
Was this helpful?
What can we do to improve the information ?