Technical FAQs

Ask a Question

Are the GV7R manual starters DIN rail mountable?

Issue:
Are the GV7R manual starters DIN rail mountable?

Product Line:
GV7 Manual Starters

Environment:
All Product Lines

Cause:
The Digest does not specify

Resolution:
The GV7R maunal starters come panel mountable from the factory.

The GV7R can be mounted on two DZ5MB201 mounting rails with the DZ5ME5.
Was this helpful?
What can we do to improve the information ?