Technical FAQs

Ask a Question

Where can I find the mounting hole information for the ATV312H018M2 thru ATV312H075M2 and ATV312H018M3 thru ATV312H075M3 drives?

Issue:
Where can I find the mounting hole information for the ATV312H018M2 thru ATV312H075M2 and ATV312H018M3 thru ATV312H075M3 drives?

Product Line:
Altivar ATV312

Environment:
All

Cause:
See the attached document and installation manual to show an example of the ATV312 drives mounting holes.
There are two 5 mm holes that are mounted on the top left side of the drive and on the bottom right side of the drive.  They are mounted about 4.76 inches apart.

Resolution:
 
Was this helpful?
What can we do to improve the information ?