Technical FAQs

Ask a Question

Does the QED2 switchboard offer Eye bolt holes for lifting?

Issue:
Does the QED2 switchboard offer Eye bolt holes for lifting?

Product Line:
PTEQP-LV EQPT (IEC & NEMA)

Environment:
Features

Cause:
Clarification

Resolution:
For QED Switchboards lless than and equal to 3000A , and Nema 1 construction, the QED SWBD's HAVE holes for the ring eye bolts used for lifting
 
Was this helpful?
What can we do to improve the information ?