Technical FAQs

Ask a Question

When did the ATV28 drive become obsolete?

Issue:
Customer would like to know when the ATV28 became obsolete.

Product line:
ATV28, Altivar 28

Environment:
All models.

Cause:
Determine age of unit, product obsolescence

Resolution:
ATV28 became obsolete in October of 2004.  The current replacement is the ATV312.  There are some differences that should be reviewed by the customer such as wiring, dimensions and ratings.
Was this helpful?
What can we do to improve the information ?