Technical FAQs

Ask a Question

When did the ATV11 drive become obsolete?

Issue:
Customer would like to know when the ATV11 became obsolete.

Product line:
ATV11, Altivar 11

Environment:
All models.

Cause:
Determine age of unit, product obsolescence

Resolution:
ATV11 became obsolete in December of 2010.  The current replacement is the ATV12.  There are some differences that should be reviewed by the customer such as wiring, dimensions and ratings. 
 
Was this helpful?
What can we do to improve the information ?