Technical FAQs

Ask a Question

When did the ATS46 soft start become obsolete?

Customer would like to know when the ATS46 became obsolete.

Product line:
ATS46, Altistart 46

All models.

Determine age of unit, product obsolescence

ATS46 became obsolete in January of 2004.  The current replacement is the ATS48.  There are some differences that should be reviewed by the customer such as wiring, dimensions and ratings. 
Was this helpful?
What can we do to improve the information ?