Technical FAQs

Ask a Question

What are the part numbers for QO115 and QO120 arc fault breakers with the plug on neutrals?

Issue:
What are the catalog numbers for QO115 and QO120 arc fault breakers with the plug on neutrals?

Product Line:
QO PCAFI breakers

Resolution:
QO115PCAFI, QO115PCAFIC and QO120PCAFI, QO120PCAFIC are the standard AFI breakers with the plug on neutral.
Dual Function catalog numbers are QO115PDF, QO120PDF, QO115VHPDF, QO120VHPDF
Was this helpful?
What can we do to improve the information ?