Technical FAQs

Ask a Question

Are the ATV12 drives rated for CT or VT applications?

Issue:
Are the ATV12 drives rated for CT or VT applications?

Product Line:
Altivar ATV12

Environment:
All

Cause:
Needs to know if the ATV12 is an constant CT or Variable CT rated drive?

Resolution:
The ATV12 is rated for both CT and VT.  
Out of the box it will be programmed for CT applications.  If you want to run a VT load you can change the motor control type from standard to Pump.

ATV12 Programming to change the motor control type
FULL menu enter
drC menu enter
Ctt = Motor control type
PerF= Performance SVSU (CT mode)
*Std= Standard VF 2 points (CT mode)
Pump= V/F for fan and pumps Variable Torque Mode (VT)
*factory default
Was this helpful?
What can we do to improve the information ?