Technical FAQs

Ask a Question

Can you adjust the IN current setting on the ATS48 while the soft starter is running?

Issue:
Can you adjust the IN current setting on the ATS48 while the soft starter is running?

Product Line:
Altistart ATS48

Environment:
All

Cause:
Wants to know if they can adjust the IN parameter while the Soft starter is running.

Resolution:
No, the ATS48 parameter settings can not be changed while the unit is a running.
Was this helpful?
What can we do to improve the information ?