Technical FAQs

Ask a Question

Wiring ABL8WPS in parallel

Issue:
Can three ABL8WPS24400 be wired in together is parallel?

Product Line:
Phaseo Power Supplies

Environment:
US Product

Cause:
Additional current capacity may be necessary than what is available from a single unit.

Resolution:
A maximum of two ABL8WP power supplies can be wired in parallel.  It is only recommended to use the exact same catalog number products for wiring in parallel or series.  See the attached document for additional information
Was this helpful?
What can we do to improve the information ?