Technical FAQs

Ask a Question

ATV71HC and ATV61HC high horse power drives can you use the side mounting holes to secure the drive?

Issue:
ATV71 and ATV61 high horse power drives can  you use the side mounting holes to secure the drive?

Product Line:
ATV71 and ATV61 HHP

Environment:
All

Cause:
Additional Mounting

Resolution:
It is not recommend using holes other than those designated for mounting specific to the drive.
Was this helpful?
What can we do to improve the information ?