Technical FAQs

Ask a Question

How can you order a full voltage bypass option on the enclosed 48U enclosed soft starters?

Issue:
How can you order a full voltage bypass option on the enclosed 48U enclosed soft starters?

Product Line:
Altistart ATS48 48U enclosed

Environment:
Enclosed 48U only

Cause:
Needs to know if they can order a full voltage bypass option on the enclosed ATS48 soft starter. Also will the unit come with an bypass selector switch?

Resolution:
Yes if you order Mod A10 this will give you the option for a full voltage bypass and there will be a bypass selector switch.
Was this helpful?
What can we do to improve the information ?